AXIS#.ENDEFAULT

Description

AXIS#. ENDEFAULT sets the default state of the software enable on power up for axes not controlled by a fieldbus (AXIS#.CMDSOURCE other than 1). Set AXIS#.ENDEFAULT to 1, to enable an axis automatically on power-up. Set AXIS#.ENDEFAULT to 0, to have the axis disabled on power-up.

Example

Queries the default state of Axis 2 on power-up:

--> AXIS2.ENDEFAULT
0

Automatically enables Axis 2 on power-up:

--> AXIS2.ENDEFAULT 1

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also AXIS#.EN , AXIS#.CMDSOURCE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.ENDEFAULT

5000h

0ah

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5012

1

5012 (0x1394)

AXIS1.ENDEFAULT

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.ENDEFAULT

5012

Unsigned8

Read/Write

-